Is necessary more than 1 ADC to measure AC voltage, Current and frequency?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is necessary more than 1 ADC to measure AC voltage, Current and frequency?

Jump to solution
1,272 Views
Braulio_Cespede
Contributor III

Hello everyone.

 

I have to work in a Project, but I not sure about this.

I think, It could be make with one, but to be sure can you tell me?.

Labels (1)
0 Kudos
Reply
1 Solution
1,013 Views
eduardo_viramon
NXP Employee
NXP Employee

Braulio,

If you plan to measure current and voltage, you need at least one ADC channel per each of those variables. Frequency is calculated from either of the current or voltage measurements (much easier based on the voltage).

The reference design in the link below has full information on how to implement a single-phase power meter. This should give you all the info you need:

http://cache.freescale.com/files/microcontrollers/doc/ref_manual/DRM133.pdf?fsrch=1&sr=11

Regards,

Eduardo V.

View solution in original post

0 Kudos
Reply
2 Replies
1,014 Views
eduardo_viramon
NXP Employee
NXP Employee

Braulio,

If you plan to measure current and voltage, you need at least one ADC channel per each of those variables. Frequency is calculated from either of the current or voltage measurements (much easier based on the voltage).

The reference design in the link below has full information on how to implement a single-phase power meter. This should give you all the info you need:

http://cache.freescale.com/files/microcontrollers/doc/ref_manual/DRM133.pdf?fsrch=1&sr=11

Regards,

Eduardo V.

0 Kudos
Reply
1,013 Views
Braulio_Cespede
Contributor III

Thanks you.

0 Kudos
Reply