The project is a 9S08QE128 project. Copying to a new project did not work. Starting the debugger the startup code runs immediately but does no stop at the jump to main (as I have been used to) . Halting shows that we are still in the copydown process although the code has been running 10 seconds or longer. This was the same experience as removing the -D for SP only initialization. I am sure this will begin to start making sense, hopefully soon.
regards Tom M.
an excerpt from the map file
*********************************************************************************************
STARTUP SECTION
---------------------------------------------------------------------------------------------
Entry point: 0x3094 (_Startup)
_startupData is allocated at 0x309F and uses 6 Bytes
extern struct _tagStartup {
unsigned nofZeroOut 2
_Range pZeroOut 0x80 128
0x100 476
_Copy *toCopyDownBeg 0xA207
} _startupData;
these are some of the records having to do with a hoped for initialization
of a const byte * array;
STRING.S1232080AC0028A39D9D.2 3171 4B 75 1 .rodata1
STRING.S12320A01B088D1A088D.3 31BC 4B 75 1 .rodata1
STRING.S12320C0E603E7026F03.4 3207 4B 75 1 .rodata1
STRING.S12320E018254D2AFAC6.5 3252 4B 75 1 .rodata1
STRING.S12321000B878A887E7D.6 329D 4B 75 1 .rodata1
STRING.S1232120F301230520B9.7 32E8 4B 75 1 .rodata1
STRING.S12321408DA7FA4520A9.8 3333 4B 75 1 .rodata1
STRING.S123216004878A88FE9F.9 337E 4B 75 1 .rodata1
STRING.S12321808BA7FB450448.10 33C9 4B 75 1 .rodata1
STRING.S12321A010898B9EFE0D.11 3414 4B 75 1 .rodata1
STRING.S12321C08B9EFE0A898B.12 345F 4B 75 1 .rodata1
STRING.S12321E00195AF009EFE.13 34AA 4B 75 1 .rodata1
STRING.S1232200018D878C9765.14 34F5 4B 75 1 .rodata1
STRING.S1232220A0419EE701AB.15 3540 4B 75 1 .rodata1
STRING.S12322400A95AF079EFF.16 358B 4B 75 1 .rodata1
STRING.S1232260B77B869E6F02.17 35D6 4B 75 1 .rodata1
STRING.S12322800025E8A7048D.18 3621 4B 75 1 .rodata1
STRING.S12322A061A825EC4F9E.19 366C 4B 75 1 .rodata1
STRING.S12322C021419EFE0989.20 36B7 4B 75 1 .rodata1
STRING.S12322E00A8745022089.21 3702 4B 75 1 .rodata1
STRING.S123230001092074C718.22 374D 4B 75 1 .rodata1
STRING.S12323204D237A239423.23 3798 4B 75 1 .rodata1
STRING.S12323400022029EE701.24 37E3 4B 75 1 .rodata1
STRING.S1232360D60121AC0022.25 382E 4B 75 1 .rodata1
STRING.S123238001068CD60121.26 3879 4B 75 1 .rodata1
STRING.S12323A0895CCF010688.27 38C4 4B 75 1 .rodata1
STRING.S12323C0019EEB029EE7.28 390F 4B 75 1 .rodata1