Is Zigbee compatible with Bluetooth?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is Zigbee compatible with Bluetooth?

5,615 Views
leecw
Contributor I
Hi,
may i know if it is possible to establish a connection with Zigbee on the transmission side and bluetooth as the receiver?
Labels (1)
0 Kudos
Reply
4 Replies

2,917 Views
Zap
Contributor I
The problem is that even if they both work on the 2.4GHz ISM band they use completely different kind of modulation. Frequency hopping over 79 1MHz channels for bluetooth and Direct Sequence for over 16 5MHz channels for Zigbee.

Piero
0 Kudos
Reply

2,917 Views
jah
Contributor I
hi guys:

in reading this brings up the question: in a area with an active zigbe network will a bluetooth signal cause interferance?

thanks!

Message Edited by jah on 2006-09-21 01:06 PM

0 Kudos
Reply

2,917 Views
Zap
Contributor I
Yes, a lot.
In my lab my Zigbee network "fight" vs. 3 bluetooth network and I can barely communicate at 1m distance. Comparing to my collegues I can say that zigbee suffer of interference much more than bluetooth does, also speacking with other engeneers they told me of severe decrese in communication when a bluetooth device enter in the area of their network. There are some paper describing coexistence with other protocol (see MC13192 section)
0 Kudos
Reply

2,917 Views
rocco
Senior Contributor II
No, It is not possible. Sorry.
0 Kudos
Reply