Is Zigbee compatible with Bluetooth?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Is Zigbee compatible with Bluetooth?

4,720 次查看
leecw
Contributor I
Hi,
may i know if it is possible to establish a connection with Zigbee on the transmission side and bluetooth as the receiver?
标签 (1)
0 项奖励
回复
4 回复数

2,022 次查看
Zap
Contributor I
The problem is that even if they both work on the 2.4GHz ISM band they use completely different kind of modulation. Frequency hopping over 79 1MHz channels for bluetooth and Direct Sequence for over 16 5MHz channels for Zigbee.

Piero
0 项奖励
回复

2,022 次查看
jah
Contributor I
hi guys:

in reading this brings up the question: in a area with an active zigbe network will a bluetooth signal cause interferance?

thanks!

Message Edited by jah on 2006-09-21 01:06 PM

0 项奖励
回复

2,022 次查看
Zap
Contributor I
Yes, a lot.
In my lab my Zigbee network "fight" vs. 3 bluetooth network and I can barely communicate at 1m distance. Comparing to my collegues I can say that zigbee suffer of interference much more than bluetooth does, also speacking with other engeneers they told me of severe decrese in communication when a bluetooth device enter in the area of their network. There are some paper describing coexistence with other protocol (see MC13192 section)
0 项奖励
回复

2,022 次查看
rocco
Senior Contributor II
No, It is not possible. Sorry.
0 项奖励
回复