Integer addition doesn t seem to work

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Integer addition doesn t seem to work

Jump to solution
4,227 Views
Juls
Contributor III

Hi

Im using codewarrior 6.3 

and a MC9s08QE32

 

When I do the following 

    cX = cM * 2;
    cY = cX + (((cM+1)*3)/5);
    cX = cY + ((sTime.cYear-i)/4);
    cY = cX - ((sTime.cYear-i)/100);
    cX = cY + ((sTime.cYear-i)/400);
    
    cY = (cX + (sTime.cYear-i));
    cX = cY + 2;
    cX %= 7;
    sTime.cDayofWeek = (char)cX;

 

where cY,cX and stime.cYear are all interger (unsigned for cyear)

Im using debugger with a openbdm

those two line doesnt change variable content

    cY = (cX + (sTime.cYear-i));
    cX = cY + 2;

but cX %=7 does work (but the final result is wrong due to 2 addition failing to add :smileyfrustrated:

 

can someone point me what im doing wrong there?

Labels (1)
0 Kudos
Reply
1 Solution
3,230 Views
Juls
Contributor III

answered myself

 

declared long int and it work now

int is not 16 bit???

 

BTW this is zeller's congruence

cM = sTime.cMonth;
    //Day of week
    if(cM == 1)
    {
        cM = 13;
        i++;
    }
    else if(sTime.cMonth == 2)
    {
        cM = 14;
        i++;
    }
    cX = sTime.cDay;
    cX += (long int)(((cM+1)*26)/10);
    cX += sTime.cYear-i;
    cX += (long int)((sTime.cYear-i)/4);
    cX += (long int)(((sTime.cYear-i)/100)*6);
    cX += (long int)((sTime.cYear-i)/400);
    
    cX %= 7;
    sTime.cDayofWeek = (char)cX;

it could be a little more compressed but it work and easy to debug

View solution in original post

0 Kudos
Reply
6 Replies
3,230 Views
Juls
Contributor III

BigMac:

i is not much of a problem since the lowest value it can get is -1

I use i when we are month jan and feb they are counted as month 13 and 14 of the year before

 

like you said you can use cY to put it in

Im using one of the formula in wiki

the lowest one they are more easy to me since we use the actual year instead of K and J

http://upload.wikimedia.org/math/d/b/7/db7eff99d21c5d7a2949c5fe68e6b771.png

 

each "part" of the formula is set into interger to remove

 

Your formala seem good (and much compressed)

im just a little incertain about

cX = (cDay + (cM + 1)*26/10 + K + K/4 + J/4 - 2*J) % 7;

Im not sure how cw will do it, will it add each floating poit one after the other if so you might get an error at the end

 

 Lundin:

the long int casting remain from when stime.cyear was still a regular int

I can remove them now :smileyvery-happy:

 

But the original problem was really

with the debugger when I was cheking

cY = (cX + (sTime.cYear-i));

cX = cY + 2;

cY didn t change at all...

both defined as int

but as long int it work so ill leave it like this :smileyvery-happy:

where cX at first was something low like 500... 16-bit is up to 65536 (/2 if signed)

Thanks

0 Kudos
Reply
3,230 Views
bigmac
Specialist III

Hello,

 

For an espression such as

 

cX = (cDay + (cM + 1)*26/10 + K + K/4 + J/4 - 2*J) % 7;

 

 

since all variables are integer, the result of any intermediate calculation will also be an integer value (with any remainder simply truncated).  Floating point values are only of consideration if one or more of the variables or constants is a floating point type.

 

Regards,

Mac

 

0 Kudos
Reply
3,231 Views
Juls
Contributor III

answered myself

 

declared long int and it work now

int is not 16 bit???

 

BTW this is zeller's congruence

cM = sTime.cMonth;
    //Day of week
    if(cM == 1)
    {
        cM = 13;
        i++;
    }
    else if(sTime.cMonth == 2)
    {
        cM = 14;
        i++;
    }
    cX = sTime.cDay;
    cX += (long int)(((cM+1)*26)/10);
    cX += sTime.cYear-i;
    cX += (long int)((sTime.cYear-i)/4);
    cX += (long int)(((sTime.cYear-i)/100)*6);
    cX += (long int)((sTime.cYear-i)/400);
    
    cX %= 7;
    sTime.cDayofWeek = (char)cX;

it could be a little more compressed but it work and easy to debug

0 Kudos
Reply
3,230 Views
Lundin
Senior Contributor IV
(long int)(expression here) There exists no situation where the above typecast is meaningful. The following cases exist for the above: - "Expression" is a small type and will not overflow. Everything is fine. - "Expression" is a small type and will overflow. The overflow has then already occured when the code reaches the typecast. The typecast DOES NOT make the operands in "Expression" 32 bit, only the result.
0 Kudos
Reply
3,230 Views
bigmac
Specialist III

Hello,

 

I am not familiar with the algorithm you are using.  The earlier code seems to differ somewhat from the later code, so my comments refer to the latter.

 

Firstly, an int is a signed 16-bit variable in CW.  I can see no particular reason why the code should overflow.  The only issue would be if  sTime.cYear were unsigned and the subtraction of i caused a negative result.

 

With the following expression:

cX += (long int)(((sTime.cYear-i)/100)*6);


may be simplified to:

cX += (sTime.cYear-i)/100*6;

 

For integer calculation, this will produce a different result than the following expression:

cX += (sTime.cYear-i)*6/100;

 

The initial expression will retain the same value for a whole century, and then change by 6.  Whereas the modified expression will increment each 16 or 17 years.  It all depends on what the algorithm requires.

 

 

Regards,

Mac

 

 

0 Kudos
Reply
3,230 Views
bigmac
Specialist III

Hello,

 

I decided to satisfy my curiosity about Zeller's congruence for the day of the week calculation.  Actually I cannot see where some of your code fits the formula given within the Wiki reference (calendars.wikia.com/wiki/Zeller's_congruence).  This includes the code previously mentioned by me.

 

Firstly, with the months of January and February considered to be the months 13 and 14 of the previous year,  and assuming that the parameter i represents the "number of years ago", incrementing this negative parameter to provide the adjustment was, at least, confusing to me.

 

Applying the formula given a little more directly, I might arrive at the following code.

 

 

#define cYear  sTime.cYear

#define cMonth sTime.cMonth

#define cDay   sTime.cDay

#define cDOW   sTime.cDayofWeek

int cM, cY, cX, J, K;

if (cMonth <= 2) {

   cM = cMonth + 12;

   cY = cYear - 1;

}

else {

   cM = cMonth;

   cY = cYear;

}

J = (cY - i) / 100;  // Century

K = (cY - i) % 100;  // Year of century (0-99)

 

cX = (cDay + (cM + 1)*26/10 + K + K/4 + J/4 - 2*J) % 7;

cDOW = (byte)cX;    // 0 = Saturday -> 6 = Friday

 

 

Regards,

Mac

0 Kudos
Reply