In Circuit Programmer - Debuger for MC9S08DZ32

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

In Circuit Programmer - Debuger for MC9S08DZ32

2,803 Views
BlueTower
Contributor II

HI! I am interested in using the MC9S08DZ32 chip cause my project involves CAN interface.

I would like to do in-circuit programming and debugging. Is there a tool available to do the job?

Labels (1)
0 Kudos
Reply
4 Replies

2,470 Views
JimDon
Senior Contributor III

You can use a USBDM. You can buy one here:

Wytec USBDM

 

0 Kudos
Reply

2,470 Views
BlueTower
Contributor II

Hi. I am interested to find out the conections on my target board. I mean which pin of the

microcontroller is used for the debugging and how is connected to the target header?

Thanks

0 Kudos
Reply

2,470 Views
JimDon
Senior Contributor III

Please refer to section 2.2 "Recommended System Connections" found in the MC8s08DZ "Data Sheet".

MC9S08DZ60.pdf

 

0 Kudos
Reply

2,470 Views
Mickey
Contributor III

Might consider this ultra-small USBDM.

 

USBDM JS16

 

Connection to target board throught standard 2-row 6-pin 2.54mm pitch.

0 Kudos
Reply