Implementing Positioning Algorithms Using Accelerometer MMA7260Q

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Implementing Positioning Algorithms Using Accelerometer MMA7260Q

21,069 Views
night_mode
Contributor I

I`ve just got my MMA7260Q accelerometer sample thanks to Freescale. Using this accelerometer i want to make a position application. My question is if somebody had implemented a position algorithm using this kind of accelerometer and where can i find some tips ?
Thanks.

--
Alban edit: FSL Part number in message subject.

Message Edited by Alban on 2007-03-28 08:48 AM

Labels (1)
0 Kudos
Reply
21 Replies

374 Views
night_mode
Contributor I
OK, thank you. Then I will try to implement this algorithm. I have some questions about this algorith: why they do 64 sample avarage in a block methode ( 64, mediation, another block of 64, mediation) this means that at 128 samples i`ll have 2 points. I think it will be better to do a rolling avarage and another thing: at some point they make a left shift with 18 and i don`t understand why they multiply the actual calculated position with a 256K value wich is a big number.
0 Kudos
Reply