Implementing Position Algorithms Using Accelerometers Document - DEMO9S08QG8

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Implementing Position Algorithms Using Accelerometers Document - DEMO9S08QG8

3,676 次查看
jmlist
Contributor I
Hello. I had a question regarding the documentation on 'Implementing Positioning Algorithm Using Accelerometers' (http://www.freescale.com/files/sensors/doc/app_note/AN3397.pdf) document. The document on page 7 refers to full source code for the application. However, there are several include files in this source code that are referenced but not included in the document or I can't find (adc.h,buzzer.h, SCItx.h). Does anyone know where these are located or if they can be?

Thanks for your help.

Justin


Message Edited by NLFSJ on 2008-10-15 04:32 PM
标签 (1)
0 项奖励
回复
3 回复数

1,888 次查看
jmlist
Contributor I
anyone? :smileyhappy:
0 项奖励
回复

1,888 次查看
Gust
Contributor I
Hola jmlist

Te puedo contestar en español? Bueno, espero que si, jeje.... el tema es que esa nota de aplicación la dan como un ejemplo de lo que se puede hacer.... mira este post

Re: Locating header files for source code used in DEMO9S08QG8


0 项奖励
回复

1,888 次查看
bigmac
Specialist III
Hello,
 
Here is the link to which I think the previous post was referring -
 
Regards,
Mac
 
0 项奖励
回复