ICS Factory Trimming

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ICS Factory Trimming

1,836 Views
Timor
Contributor I

Hi,

 

I want to work with the factory trimming values but, as far as i understand, those values are not loaded into the ICS trim registers if BDM is active.

This means that during development, while i am working with a debugger, i can not get the device to run with the factory trim values.

 

Is there a way to read and load the factory trim values into the ICS trim registers?

 

I am working with CW10.6, MC9S08PA8, P&E Multilink debugger

 

Thanks,

Timor

Labels (1)
0 Kudos
Reply
2 Replies

1,700 Views
w_tension
Contributor III

CodeWarrior load the TRIM value by default when debug, and it's optional, you can turn off.

User should load by himself, example projects do this, too.

QQ截图20160901090221.png

0 Kudos
Reply

1,700 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Hi

please also check this application note for more information about the ICS and the clock option on the S08

Clock Options on the HC9S08 Family

Regards

Vicente Gomez

0 Kudos
Reply