ICS Factory Trimming

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ICS Factory Trimming

1,872件の閲覧回数
Timor
Contributor I

Hi,

 

I want to work with the factory trimming values but, as far as i understand, those values are not loaded into the ICS trim registers if BDM is active.

This means that during development, while i am working with a debugger, i can not get the device to run with the factory trim values.

 

Is there a way to read and load the factory trim values into the ICS trim registers?

 

I am working with CW10.6, MC9S08PA8, P&E Multilink debugger

 

Thanks,

Timor

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,736件の閲覧回数
w_tension
Contributor III

CodeWarrior load the TRIM value by default when debug, and it's optional, you can turn off.

User should load by himself, example projects do this, too.

QQ截图20160901090221.png

0 件の賞賛
返信

1,736件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

Hi

please also check this application note for more information about the ICS and the clock option on the S08

Clock Options on the HC9S08 Family

Regards

Vicente Gomez

0 件の賞賛
返信