ICS Factory Trimming

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ICS Factory Trimming

1,794 次查看
Timor
Contributor I

Hi,

 

I want to work with the factory trimming values but, as far as i understand, those values are not loaded into the ICS trim registers if BDM is active.

This means that during development, while i am working with a debugger, i can not get the device to run with the factory trim values.

 

Is there a way to read and load the factory trim values into the ICS trim registers?

 

I am working with CW10.6, MC9S08PA8, P&E Multilink debugger

 

Thanks,

Timor

标签 (1)
0 项奖励
回复
2 回复数

1,658 次查看
w_tension
Contributor III

CodeWarrior load the TRIM value by default when debug, and it's optional, you can turn off.

User should load by himself, example projects do this, too.

QQ截图20160901090221.png

0 项奖励
回复

1,658 次查看
vicentegomez
NXP TechSupport
NXP TechSupport

Hi

please also check this application note for more information about the ICS and the clock option on the S08

Clock Options on the HC9S08 Family

Regards

Vicente Gomez

0 项奖励
回复