ICG oscillator operation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ICG oscillator operation

1,315件の閲覧回数
BobMac
Contributor I

Hi Everybody;

 

 With a new (non programmed) 9S08AC60 and crystal (4 MHz), caps, resistor connected to xtal & extal pins. On the application of power, 5V dc., is the ICG crystal oscillator supposed to run? Always/ sometimes/ never? 

 

Regards, Bob

ラベル(1)
0 件の賞賛
返信
1 返信

1,182件の閲覧回数
bigmac
Specialist III

Hello Bob,

 

After POR, the default operating mode for the ICG module will be FEI.  The crystal oscillator will be inoperative.  You will then need to set ICGC1 to enable the oscillator, and to switch to FEE mode.  Refer to the datasheet, section 10.5.3, Example #2 for the required procedure.

 

Regards,

Mac

 

0 件の賞賛
返信