Hello,
I am using I2C module in MC9S08AW32 to communicate with Freescale MMA7455L accelerometer. I am able to communicate with the accelerometer and read the values from it.
But sometimes, I2C bus hangs up with SCL line high and SDA line low. After this state, I am not able to communicate with the accelerometer. Only when I cutoff the power to accelerometer for few seconds, it starts communicating again. How is that I can reset the I2C bus without resetting the whole board.
regards
Vishu
 
					
				
		
Vishu,
Had a similar problem in the past with an IIC master on the QG4/8. Turned out I was not polling the BUSY flag at the start of a transmission, and sometimes on back-to-back transmissions the new one would start before the signalling of the stop condition of the previous one was done(in software, we clear MST to signal a stop but don't poll until it's done). This would cause the master to hang on the subsequent transmission.
While I'm not sure of the IIC module on the AW32, I suspect its similar. Before each IIC access, try to poll the BUSY flag until it's clear before sending a start condition.
 
					
				
		
Vishu,
I believe you will find this is a missed ACK of some type. I had a very similar problem a couple of years ago using a GP32 and ended up bit banging the interface so I could detect the problem and correct it in firmware since the module in the GP32 would just hang with no possible recovery except a power cycle.
You can probably catch this on a scope if you trigger on the rising edge of the SDA line and inspect the events after the final trigger up until the data stops.
Good Luck,
Peter House
Hi Peter,
Thanks for your response.
One more thing I would like to know is, even if I correct my firmware to not to miss the ACK, there might be situations in the field where the I2C bus may hang up.
What I read in many forums is that if we send 9 clock pulses followed by a stop signal on the I2C bus, it will unhang the bus.
Since I am using the AW32 I2C module, I cannot use the pins directly to send 9 clocks.
Is there any other way to unhang the bus?
Thanks and Regards
Vishu
 
					
				
		
Vishnu,
I could not get it to work on the GP32 and had to resort to replacing the module with my own code so I could clear the bus. It is not very difficult and does not take a lot of CPU time to run.
I did spend a lot of time sending scope shots and such to Freescale only to have them blame the issue on the i2c chip or my code. Funny, when I replaced their module it worked and is still working flawlessly! I use a lot of Freescale CPUs and this module is the only one which has ever given me this much trouble.
Peter