How to soft-reset USB MSD?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to soft-reset USB MSD?

1,800件の閲覧回数
leesp
Contributor I

I am implementing a USB MSD Bootloader using MC9s08JM32.

After the bootloading process, the MCU will re-enumerate as a MSD device.

I would like to be able to send a command to soft-reset the MSD device at this point. My application is designed in such way that, if I soft-reset it, it will enter User code and enumerate as a HID device.

 

Question: How can I soft-reset a MSD device? By sending raw SCSI command? I do not want to implement a composite USB device, so soft-resetting by sending command to HID endpoint is out of the question.

ラベル(1)
0 件の賞賛
返信
1 返信

1,445件の閲覧回数
david_diaz
NXP Employee
NXP Employee

Hello Lee,

What do you mean with soft-reset?

In case you are pretending to restart the USB module, you may refer to the following recommendations:

1.Set the USBRESET bit from the USB Control Register 0 (USBCTL0).

or

2. Set the USBPU bit from the USB Control Register 0 (USBCTL0).

Please find more detailed information at the MC9S08JM32 datasheet , especially at chapter 17.3.1:

USB reset.jpg

I hope this information will be useful for you.

If I misunderstood your question, feel free to let me know.  I will be glad to help.

Have a great day.

David Diaz.

0 件の賞賛
返信