How to read the contents in EEPROM of mask version of MC68HC08AB16?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to read the contents in EEPROM of mask version of MC68HC08AB16?

2,974件の閲覧回数
ygning
Contributor I
Hi,Dears,
Do you tell me how to read the contents in EEPROM of Mask version of MC68HC08AB16.It is appriciated for your reply.
 
Best Regards,
 
Ning
ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,483件の閲覧回数
ygning
Contributor I
Hi,Dears,
Thanks for your reply.
I have the device's eight-byte security key when entering monitor mode,and I can read the contents of Mask device of AB16.But I can not read the contents of EEPROM.I read the datasheet of MC68HC08AB16,and I want to know whether the security code of EEPROM is the same as the device security code.
Thanks.
 
Best regards,
 
Ning
0 件の賞賛
返信

1,483件の閲覧回数
rocco
Senior Contributor II
Hi, Ning:

Yes, there is only one security code, and if you can read the mask-rom, then you have the correct code.

You should be able to read the EEprom the same way as you would read the rom or ram contents. The addresses that you would use should be the only difference. Could the problem be with the program you are using to read with?
0 件の賞賛
返信

1,483件の閲覧回数
rocco
Senior Contributor II
Hi, Ning:

Whether or not you can read the EEProm will depend on how the mask rom in the device was initially configured, and whether or not you have the eight-byte security key.

You can read the EEProm in monitor mode without the security key if:
1) Extended security was not enabled in the mask-rom, AND
2) EEProm security was also not enabled (EEMONSEC=0 in mask option register B).

In either case, the EEProm would be accessed in monitor mode. If either of these security features were enabled, then you will need the device's eight-byte security key when entering monitor mode in order to access the EEProm.
0 件の賞賛
返信