How to read suffix of part nr for example 68HC711K4CFN4 replaceable by CFN3?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to read suffix of part nr for example 68HC711K4CFN4 replaceable by CFN3?

1,876 Views
cor_van_de_wate
Contributor I
Sorry if this is documented here already, I tried several searches and could not find any
difference in specs between a processor part nr
68HC711K4CFN3 and the (original) CFN4 that is in the controller.
This is for an Electric Vehicle (US Electricar) which has a 50 kW 3-phase AC drivetrain made by Hughes,
unfortunately information is scarce and the CFN4 parts are hard to find,
but CFN3 are plentiful.
Anybody able to enlighten me?
Thanks,
Cor.
Labels (1)
0 Kudos
Reply
2 Replies

1,072 Views
kef
Specialist I
The number in the HC11 part name suffix means max bus clock frequency in MHz. CFN3 - up to 3MHz bus clock (up to 12MHz oscilator frequency), CFN4 - up to 4MHz bus clock(up to 16MHz oscilator frequency).
0 Kudos
Reply

1,072 Views
cor_van_de_wate
Contributor I
That clarifies why I could not see any difference in functional description.
The K4 family datasheet is missing this information.
Thank you for clearing this up,
Cor.
0 Kudos
Reply