How to read suffix of part nr for example 68HC711K4CFN4 replaceable by CFN3?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to read suffix of part nr for example 68HC711K4CFN4 replaceable by CFN3?

1,774件の閲覧回数
cor_van_de_wate
Contributor I
Sorry if this is documented here already, I tried several searches and could not find any
difference in specs between a processor part nr
68HC711K4CFN3 and the (original) CFN4 that is in the controller.
This is for an Electric Vehicle (US Electricar) which has a 50 kW 3-phase AC drivetrain made by Hughes,
unfortunately information is scarce and the CFN4 parts are hard to find,
but CFN3 are plentiful.
Anybody able to enlighten me?
Thanks,
Cor.
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

970件の閲覧回数
kef
Specialist I
The number in the HC11 part name suffix means max bus clock frequency in MHz. CFN3 - up to 3MHz bus clock (up to 12MHz oscilator frequency), CFN4 - up to 4MHz bus clock(up to 16MHz oscilator frequency).
0 件の賞賛
返信

970件の閲覧回数
cor_van_de_wate
Contributor I
That clarifies why I could not see any difference in functional description.
The K4 family datasheet is missing this information.
Thank you for clearing this up,
Cor.
0 件の賞賛
返信