How to load a program into my mc9s08qg8 evalboard

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to load a program into my mc9s08qg8 evalboard

2,543件の閲覧回数
srinivasakiran
Contributor I

Hai guys,

 Recently i attened a free scale seminar and got the mc9s08qg8 demo board along with the codewarrior ide free with it. It is a 8 bit controller board.I tried running the sample applications provied by them, but i could not flash the code into the target. I am new bee to use code warrior and to free scale controllers. I am here by attaching the snap shots the command window that is displayed the error. I request you to  help me to load code into the board.

 

Thanks and advance,

kiran. 

mc9.JPG

Message Edited by t.dowe on 2009-09-08 09:30 AM
ラベル(1)
0 件の賞賛
返信
1 返信

1,247件の閲覧回数
GrungeRey
Contributor I

Hi srinivasakiran,

 

 

Try changing the the Device and connection, it should match the device.

In default it is maked as MC9S08QE128, if you are using MC9S08QG8 then replace it.

 

see files attached for steps.

 

Hope this helps you...

 

answer to srinivasakiran.doc

Message Edited by t.dowe on 2009-10-07 09:11 AM
0 件の賞賛
返信