How to implement TinyOS on Freescale platform

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to implement TinyOS on Freescale platform

2,550件の閲覧回数
Yetao
Contributor I

Hoi guys,

 :smileyhappy:

I am going to implement TinyOS on the latest Freescale MC1322X platform ?

 

Is anybody here family with MC1322X platform or had experience before of implementing TinyOS on MCS9S08GT60A series platform ?

 

Thanks in advance!

 

Yetao

ラベル(1)
0 件の賞賛
返信
1 返信

1,259件の閲覧回数
nonarKitten
Contributor II

Good luck with the MC13224 - speaking from experience, I went through the effort of porting FreeRTOS to it. The built-in interrupt handling is painfully slow and creates a bad stackframe, so you either have to work around that and live with the speed, or implement your own IRQ routine and dump 99% of the ROM (the route I ended up taking).

 

You'll have a tougher time as TinyOS uses nesC and the GCC tool-chain. Not much success has been made with reverse engineering the hardware and ROM, but these guys would be a great start: http://mc1322x.devl.org/. TinyOS looks pretty cool, and it would be nice to have something like Mat'e available for the MC13224, but I have zero familiarity with nes

0 件の賞賛
返信