How to generate interface receive SPI or SCI and exit with BDC to program MC9S08AC16?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to generate interface receive SPI or SCI and exit with BDC to program MC9S08AC16?

1,212 次查看
enriqueperelis
Contributor I

Hello.
I need to make a hardware that allows a Raspberry to modify the firmware programmed in a MC9S08AC16.

I cannot incorporate a commercial development board.

Is there a dedicated integrated circuit or published program to incorporate it into another microcontroller that is the link between Raspberry and MC9S08AC16, that receives data through SPI or SCI and comes out with the BDC protocol?

标记 (2)
0 项奖励
回复
1 回复

1,199 次查看
vicentegomez
NXP TechSupport
NXP TechSupport

Do you want a serial bootloader?

 

If this is the case, please check the an2295

https://www.nxp.com/docs/en/application-note/AN2295.pdf

 

I hope this will help you

Regards

Vicente G

0 项奖励
回复