How to generate 2MHz output clock on S08 mcu?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to generate 2MHz output clock on S08 mcu?

跳至解决方案
1,459 次查看
mehdializadeh
Contributor II

Hi,

I am using mc9s08dz96 microcontroller with 8 MHz external clock osc.

I want to generate 2MHz output clock on the port PTA0 of microcontroller for another IC? I want to ask how is it done?

Thank you.

0 项奖励
回复
1 解答
1,446 次查看
vicentegomez
NXP TechSupport
NXP TechSupport

What is your bus clock frequency ?

 

If you set the bus clock to 4 MHz 

 

something like this

 

/* ### MC9S08DZ128_100 "Cpu" init code ... */
/* PE initialization code after reset */
/* Common initialization of the write once registers */
/* SOPT1: COPT=0,STOPE=0,SCI2PS=0,IIC1PS=0,??=0,??=0,??=0 */
setReg8(SOPT1, 0x00U);
/* SOPT2: COPCLKS=0,COPW=0,??=0,ADHTS=0,??=0,MCSEL=0 */
setReg8(SOPT2, 0x00U);
/* SPMSC1: LVWF=0,LVWACK=0,LVWIE=0,LVDRE=1,LVDSE=1,LVDE=1,??=0,BGBE=0 */
setReg8(SPMSC1, 0x1CU);
/* SPMSC2: ??=0,??=0,LVDV=0,LVWV=0,PPDF=0,PPDACK=0,??=0,PPDC=0 */
setReg8(SPMSC2, 0x00U);
/* System clock initialization */
/*lint -save -e923 Disable MISRA rule (11.3) checking. */
if (*(uint8_t*)0xFFAFU != 0xFFU) { /* Test if the device trim value is stored on the specified address */
MCGTRM = *(uint8_t*)0xFFAFU; /* Initialize MCGTRM register from a non volatile memory */
MCGSC = *(uint8_t*)0xFFAEU; /* Initialize MCGSC register from a non volatile memory */
}
/*lint -restore Enable MISRA rule (11.3) checking. */
/* MCGC2: BDIV=1,RANGE=1,HGO=0,LP=0,EREFS=0,ERCLKEN=1,EREFSTEN=0 */
setReg8(MCGC2, 0x62U); /* Set MCGC2 register */
/* MCGC3: DIV32=1 */
setReg8Bits(MCGC3, 0x10U);
/* MCGC1: CLKS=0,RDIV=3,IREFS=0,IRCLKEN=1,IREFSTEN=0 */
setReg8(MCGC1, 0x1AU); /* Set MCGC1 register */
/* MCGC3: LOLIE=0,PLLS=0,CME=0,DIV32=1,VDIV=1 */
setReg8(MCGC3, 0x11U); /* Set MCGC3 register */
/* MCGT: ??=0,??=0,DMX32=0,??=0,??=0,??=0,??=0,DRST_DRS=0 */
setReg8(MCGT, 0x00U); /* Set MCGT register */
while(MCGSC_IREFST != 0U) { /* Wait until external reference is selected */
}
while((MCGSC & 0x0CU) != 0x00U) { /* Wait until FLL clock is selected as a bus clock reference */

 

and after you need to set 

the MCSEL to 01 

I hope this will help you.

在原帖中查看解决方案

2 回复数
1,423 次查看
mehdializadeh
Contributor II

Thank you so much, the problem solved with setting MCSEL to 01.

0 项奖励
回复
1,447 次查看
vicentegomez
NXP TechSupport
NXP TechSupport

What is your bus clock frequency ?

 

If you set the bus clock to 4 MHz 

 

something like this

 

/* ### MC9S08DZ128_100 "Cpu" init code ... */
/* PE initialization code after reset */
/* Common initialization of the write once registers */
/* SOPT1: COPT=0,STOPE=0,SCI2PS=0,IIC1PS=0,??=0,??=0,??=0 */
setReg8(SOPT1, 0x00U);
/* SOPT2: COPCLKS=0,COPW=0,??=0,ADHTS=0,??=0,MCSEL=0 */
setReg8(SOPT2, 0x00U);
/* SPMSC1: LVWF=0,LVWACK=0,LVWIE=0,LVDRE=1,LVDSE=1,LVDE=1,??=0,BGBE=0 */
setReg8(SPMSC1, 0x1CU);
/* SPMSC2: ??=0,??=0,LVDV=0,LVWV=0,PPDF=0,PPDACK=0,??=0,PPDC=0 */
setReg8(SPMSC2, 0x00U);
/* System clock initialization */
/*lint -save -e923 Disable MISRA rule (11.3) checking. */
if (*(uint8_t*)0xFFAFU != 0xFFU) { /* Test if the device trim value is stored on the specified address */
MCGTRM = *(uint8_t*)0xFFAFU; /* Initialize MCGTRM register from a non volatile memory */
MCGSC = *(uint8_t*)0xFFAEU; /* Initialize MCGSC register from a non volatile memory */
}
/*lint -restore Enable MISRA rule (11.3) checking. */
/* MCGC2: BDIV=1,RANGE=1,HGO=0,LP=0,EREFS=0,ERCLKEN=1,EREFSTEN=0 */
setReg8(MCGC2, 0x62U); /* Set MCGC2 register */
/* MCGC3: DIV32=1 */
setReg8Bits(MCGC3, 0x10U);
/* MCGC1: CLKS=0,RDIV=3,IREFS=0,IRCLKEN=1,IREFSTEN=0 */
setReg8(MCGC1, 0x1AU); /* Set MCGC1 register */
/* MCGC3: LOLIE=0,PLLS=0,CME=0,DIV32=1,VDIV=1 */
setReg8(MCGC3, 0x11U); /* Set MCGC3 register */
/* MCGT: ??=0,??=0,DMX32=0,??=0,??=0,??=0,??=0,DRST_DRS=0 */
setReg8(MCGT, 0x00U); /* Set MCGT register */
while(MCGSC_IREFST != 0U) { /* Wait until external reference is selected */
}
while((MCGSC & 0x0CU) != 0x00U) { /* Wait until FLL clock is selected as a bus clock reference */

 

and after you need to set 

the MCSEL to 01 

I hope this will help you.