How to connect two LIN ports  with cable together

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to connect two LIN ports  with cable together

2,066件の閲覧回数
baonguyen
Contributor I
Dear everybody,
 
       I am novice in embedded programmation. I have 2 HC08GZ60 boards and I want to connect them with LIN cable. But could anyone can show me the way (in form of a picture, for example) to connect them using con1 or con2 ports? Each conx has 4 pin, so what pin do we have to use?
 
Thanks a lot
Best regard
 
ラベル(1)
0 件の賞賛
返信
1 返信

1,130件の閲覧回数
Nabla69
Contributor V
Evening Bao,
 
Just need to connect all pin 1 to pin 1, 2 to 2....
It's a bus and there is nothing to cross-over.
 
Only 2 pins are really useful:
 - Blue wire, square pin, top left when you look at your board = LIN BUS
 - Black Wire, square pin, bottom right when you look at your board = GROUND.
 
You can also use the connector to distribute power like VBAT, that's how it's cabled:
 - Red wire, hexagonal pin, top right when you look at your board = VBAT
 
Didn't you get a Molex cable like that in the LIN KIT ???
 
Hope this helps,
Alvin.
0 件の賞賛
返信