How to Add the protection to internal Flash ??

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to Add the protection to internal Flash ??

ソリューションへジャンプ
3,194件の閲覧回数
Harlen_CHen
Contributor I

Hello,

We use the MC908GT16 for 3 years. Currently, we find the internal flash to be changed. The program can not run correctly. Originally, we dont add the protection to the internal Flash. We want to know:

1. How to add protection to the entire Flash?

2. If protection , We can read the program of Flash? How to read?

3. If protection, the Flash can be re-program ?

 

Best regards

harlen

ラベル(1)
0 件の賞賛
返信
1 解決策
2,123件の閲覧回数
peg
Senior Contributor IV

Hello Harlen,

 

What you want can be achieved by using Flash block protection.

See section 4.4.6 of the manual. Maybe look at the GT16A manual for a better description.

You just programme NVPROT with the appropriate value and that's it. ($BE)

 

This only provides protection from internal access.

When you connect via a BDM adapter the software will un-protect the flash so it may be then modified.

Note that this un-protecting can only be done through the BDM.

 

If still not clear on this perhaps you can narrow down your area of concern.

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,124件の閲覧回数
peg
Senior Contributor IV

Hello Harlen,

 

What you want can be achieved by using Flash block protection.

See section 4.4.6 of the manual. Maybe look at the GT16A manual for a better description.

You just programme NVPROT with the appropriate value and that's it. ($BE)

 

This only provides protection from internal access.

When you connect via a BDM adapter the software will un-protect the flash so it may be then modified.

Note that this un-protecting can only be done through the BDM.

 

If still not clear on this perhaps you can narrow down your area of concern.

 

0 件の賞賛
返信
2,123件の閲覧回数
OmarAI
Contributor I
I've read your post but can't understand it completely....can you be more specific?
0 件の賞賛
返信