How long is it valid for FLL lock?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How long is it valid for FLL lock?

1,099件の閲覧回数
w_lingjun
Contributor III

Hi All,

I am having problem when I use a demo routine to set FEE mode for S9KEAZ128.

The bold line is to wait for FLL to lock, and it takes about 26ms, I think it is too long for initialization.

How long is it valid for FLL lock?

20.5.3 Initializing FEE mode

The following code segment demonstrates setting ICS to FEE mode.
Example: 20.5.3.1   FEE mode initialization routine
/* the following code segment demonstrates setting the ICS to FEE mode generating a 40MHZ core clock frequency using an external 8MHz crystal */

OSC_CR = 0x96; // high-range, high-gain oscillator selected

while ((OSC_CR & OSC_CR_OSCINIT_MASK) == 0); // wait until oscillator is ready

ICS_C2 = 0x20; // BDIV=divide by 2 – use default until clock dividers configured

ICS_C1 = 0x18; // 8MHz external reference clock/256 as source to FLL

while ((ICS_S & ICS_S_IREFST_MASK) == 1); // wait for external source selected

while ((ICS_S & ICS_S_LOCK_MASK) == 0); // wait for FLL to lock

SIM_CLKDIV = 0x01100000; // core clock = ICSOUT/1 and bus clock = core clock/2

ICS_C2 = 0x00; // BDIV=divide by 1 – allows max core and bus clock frequencies

タグ(1)
0 件の賞賛
返信
0 返答(返信)