Help with using TSN from 1028ardb via putty

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Help with using TSN from 1028ardb via putty

1,832件の閲覧回数
nhanthanh
Contributor I

I want to use qbv feature on putty.

0 件の賞賛
返信
1 返信

1,732件の閲覧回数
CarrieDuoduo
Contributor I

To use the TSN (Time-Sensitive Networking) and QBV (Quality of Service Basic Mode) features on the 1028ardb board via PuTTY, you first need to establish a serial connection between your computer and the board. Here are the steps to do so:

  1. Connect the serial cable to your computer's serial port or USB-to-serial adapter.

  2. Open PuTTY and go to the "Serial" category under the "Connection" tab.

  3. Under the "Serial line" field, enter the serial port number that corresponds to your serial connection (e.g. COM1 or /dev/ttyS0).

  4. Set the baud rate to 115200 (or whatever baud rate is specified by the 1028ardb board manual).

  5. Click on the "Open" button to open the serial connection.

Once you have established the serial connection, you can access the TSN and QBV features by using the command-line interface of the 1028ardb board. You may refer to the board's manual for the specific commands needed to enable and configure these features.

Hope help.

Life-long learning
0 件の賞賛
返信