Help needed. To generate PWM on a freescale microcontroller

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Help needed. To generate PWM on a freescale microcontroller

3,825件の閲覧回数
Ram_newbee
Contributor I

Hi all

Am using Freescale Micro controller MC9S08SH8. Iam trying to create a PWM using this controller. Though I have carefully set all the registers related to PWM, Am still unable to generate PWM on this.

The main task was to create a edge aligned PWM on all channels of each PWM.
also am using internal oscillator it has.

Can any one give me some example C Codes for the same or try correcting my code.

Tools am using: Codewarrior suite with P&E Programmer
Controller: MC9S08SH8 20pin


Any kind of help is greatly appreciated

Thanks!

 

 

My Code

 

#include <hidef.h> /* for EnableInterrupts macro */#include "derivative.h" /* include peripheral declarations */void main(void) {  EnableInterrupts; /* enable interrupts */     //TIMER1 CH0 n CH1          TPM1SC=0b01001000;     TPM1C0SC=0b00101000;  //Edge aligned pwm with high true pulses      TPM1C1SC=0b00101000;      TPM1MOD=400;     TPM1C0V=400;     TPM1C1V=400;          //TIMER2 CH0 n CH1        TPM2SC=0b01001000;     TPM2C1SC=0b00100100; //Edge aligned pwm with low true pulses      TPM2C0SC=0b00100100;     TPM2MOD=400;     TPM2C1V=400;     TPM2C0V=400;while(1){TPM1C0V=300;TPM1C1V=300;TPM2C1V=300;TPM2C0V=300;}   }
ラベル(1)
0 件の賞賛
返信
5 返答(返信)

2,838件の閲覧回数
bigmac
Specialist III

Hello, and welcome to the forum.

 

I have successfully used the assembly equivalent of the following code to generate antiphase PWM signals to directly drive a piezo buzzer device.  The code was tested on a '9S08SE8, but should also work for the device you are using.

 

// TPM1 MODULE:// Generates 4 kHz PWM push-pull output from Ch0 and Ch1 for piezo.// Overflow period: 250 us#ifdef  LOW_TRIM#define TPM1MODval  999     //(1) (250*4.00 - 1)  4.00 MHz bus#else#define TPM1MODval  1249    //(2) (250*5.00 - 1)  5.00 MHz bus#endif#define TPM1SCval   0x08 /* 0b00001000  TPM1SC register                              |||||+++- PS     Prescaler divisor 1                              |||++---- CLKS   Bus rate clock                              ||+------ CPWMS  Edge aligned PWM mode                              |+------- TOIE   No overflow interrupt                              +-------- TOF    Read only flagNote: Clearing TPM1SC register will disable TPM1 module*/#define TPM1C0SCval 0x28 /* 0b00101000  TPM1C0SC register                              ||||++--- ELS0    High true output pulses                              ||++----- MS0     PWM mode (edge aligned)                              |+------- CH0IE   No channel interrupt                              +-------- CH0F    Read only flag*/#define TPM1C1SCval 0x2C /* 0b00101100  TPM1C1SC register                              ||||++--- ELS1    Low true output pulses                              ||++----- MS1     PWM mode (edge aligned)                              |+------- CH1IE   No channel interrupt                              +-------- CH1F    Read only flagNote: Clearing TPM1CnSC register will disable PWM output*//***************************************************************/// TPM1 module initialisationvoid TPM1_init( void){   TPM1MOD = TPM1MODval;   TPM1SC  = 0;             // Initially disable module}/***************************************************************/// TURN AUDIBLE BEEP ON/OFF#define DUTY_50   (TPM1MODval+1)/2 // PWM duty cycle 50%void BUZZ_ON( void){   TPM1SC   = TPM1SCval;    // Enable TPM1 module   TPM1C0SC = TPM1C0SCval;  // Enable TPM1 output Ch0   TPM1C1SC = TPM1C1SCval;  // Enable TPM1 output Ch1   TPM1C0V  = DUTY_50;      // PWM duty cycle 50%   TPM1C1V  = DUTY_50;      // PWM duty cycle 50%}void BUZZ_OFF( void){   TPM1C0SC = 0;   TPM1C1SC = 0;}

 

 

Regards,

Mac

 

0 件の賞賛
返信

2,838件の閲覧回数
bigmac
Specialist III

Hello,

 

I discovered that the code I previously posted was from an early version of the firmware.  The later version is different, presumably because of problems experienced during debugging.  Only the BUZZ_ON() function is affected, and the modified code follows.

 

void BUZZ_ON( void){   TPM1SC   = 0;            // Disable TPM1 module   TPM1C0V  = DUTY_50;      // PWM duty cycle 50%   TPM1C1V  = DUTY_50;      // PWM duty cycle 50%   TPM1SC   = TPM1SCval;    // Enable TPM1 module   TPM1C0SC = TPM1C0SCval;  // Enable TPM1 output Ch0   TPM1C1SC = TPM1C1SCval;  // Enable TPM1 output Ch1}

 

I now recall that the channel register settings did not update unless the TPM module was first disabled.  I apologise for any confusion.

 

Regards,

Mac

0 件の賞賛
返信

2,838件の閲覧回数
Ram_newbee
Contributor I

Hey thanks again for the update. I have changed the code to suit my prupose and since I dont need to use it for buzzer, I didn't encounter any problem. I have a few basic doubts.

 

What does this do?

 

#ifdef  LOW_TRIM
#define TPM1MODval  999     //(1) (250*4.00 - 1)  4.00 MHz bus
#else
#define TPM1MODval  1249    //(2) (250*5.00 - 1)  5.00 MHz bus
#endif

 

And also How can I generate PWMs with various frequencies. I mean what register should I vary if I have to change the frequency of my PWM.

 

Thanks!

 

 

0 件の賞賛
返信

2,838件の閲覧回数
bigmac
Specialist III

Hello,

 

The PWM period is determined by the modulo setting, within the TPMxMOD register.  Assuming the TPM module clock is sourced from the bus, and usually with a prescaler division by 1 for PWM, the number of bus cycles per PWM period will be one more than the modulo value.

 

The purpose of the preprocessor conditional #defines is to allow for PWM period calibration, in this case for a 250 microseconds period, for two different trim settings associated with the internal reference of the ICS module (using FEI mode).

 

Regards,

Mac

 

0 件の賞賛
返信

2,838件の閲覧回数
Ram_newbee
Contributor I

Thank You bigmac, I ll try to work it out and will update you accordingly

 

Regards

0 件の賞賛
返信