Help i2c protocol

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Help i2c protocol

Jump to solution
3,141 Views
Eliezer
Contributor I

Hello, does anyone know how to set up a communication routine i2c register but without using the microcontroller without the SDA end SCL pins, only with common pins

Labels (1)
0 Kudos
Reply
1 Solution
2,674 Views
rocco
Senior Contributor II

And here is the macro file.

View solution in original post

0 Kudos
Reply
4 Replies
2,674 Views
rocco
Senior Contributor II

Hi Eliezer,

 

Are you asking for code to "bit-bang" the I2C protocol?  If so, do you need C or assembly language? Are you using an HC08 or S08?

 

I you are using assembly language on an 08, I've implemented I2C as a bunch of macros (originally for the HC05). It uses a lot of in-line code to try to be fast, but it is still rather slow. Bit-timing may be an issue, as you may need to pad some macros with NOPs on the faster S08s.

0 Kudos
Reply
2,674 Views
Eliezer
Contributor I

Hello Rocco.

Yes, I need a code in C for the I2C protocol. I am using KA8 the RS08 family, but I canbe what you

have, already helps me a lot.

Grateful.

0 Kudos
Reply
2,674 Views
rocco
Senior Contributor II

Hi Eliezer,

 

The KA8 is neither an S08 or an HC08, but an RS08, so the assembly language code may not work (I have never used an RS08, as I consider them brain-damaged.

 

But here is my I2C macro file anyway. IYou use it by stringing I2C commands together, such as this routine from an HC08 project:

;
;
; Read all just the motor limit parameters from the EEPROM,
; from the page pointed to by 'ParameterPage'. The parameters
; we need to read are 'MinPosition' and 'MaxPosition'.
;
ParamLoadLimits:
 EE_READ ParameterPage,#(MinPosition-EEP_Start),EER_ERR2
    ;node page, byte in EEPROM, error exit
;
 EE_BYTE_IN  ;get a data byte from EEPROM
 EE_ACK   ;ACK it to continue
 sta MinPosition ;store the data byte
;
 EE_BYTE_IN  ;get a data byte from EEPROM
 EE_ACK   ;ACK it to continue
 sta MinPosition+1 ;store the data byte
;
 EE_BYTE_IN  ;get a data byte from EEPROM
 EE_ACK   ;ACK it to continue
 sta MinPosition+2 ;store the data byte
;
 EE_BYTE_IN  ;get a data byte from EEPROM
 EE_ACK   ;ACK it to continue
 sta MaxPosition ;store the data byte
;
 EE_BYTE_IN  ;get a data byte from EEPROM
 EE_ACK   ;ACK it to continue
 sta MaxPosition+1 ;store the data byte
;
 EE_BYTE_IN  ;get a data byte from EEPROM
 EE_NAK   ;NAK it to make it stop
 sta MaxPosition+2 ;store the data byte
;
; done reading bytes
;
 EE_STOP   ;and issue the stop sequence.
;
 jsr SetLimits ;update the DSP on the situation
 clc   ;clear carry
 rts   ;return happy with carry clear
;
;
; EEPROM error routine for a Read of limit parameters.
;
EER_ERR2:
 EE_STOP   ;drop the EEPROM
 ErrLog E_EEPRMread ;"EEPROM Read Error"
 sec   ;set carry
 rts   ;return empty handed with carry set

 

0 Kudos
Reply
2,675 Views
rocco
Senior Contributor II

And here is the macro file.

0 Kudos
Reply