Hello, I need to find eagle library for microcontroller M... - MC9S08LC60

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hello, I need to find eagle library for microcontroller M... - MC9S08LC60

Jump to solution
4,489 Views
Jura
Contributor I
Hello, I need to find eagle library for microcontroller MC9S08LC60 package 64-Pin LQFP and 80-pin LQFP. Thanks for help! Jiri
 
 
 
 
 
 
 
 
 
 
Added p/n to subject.


Message Edited by NLFSJ on 2008-06-13 08:17 AM
Labels (1)
0 Kudos
Reply
1 Solution
1,428 Views
protoease
Contributor II
You could just make one, its fairly easy to do- start by making a symbol for each type, 64 and 80 pin.  Then you can just copy in the package from the smd-ipc family and map the symbol pins to the footprint pins.

I can help you make a library part for this part if you want.  I've made my own library that so far contains the QG, QE, JM, AW/AC.  Will continue to add to it and make it available to everyone if desired.


Aaron

View solution in original post

0 Kudos
Reply
1 Reply
1,429 Views
protoease
Contributor II
You could just make one, its fairly easy to do- start by making a symbol for each type, 64 and 80 pin.  Then you can just copy in the package from the smd-ipc family and map the symbol pins to the footprint pins.

I can help you make a library part for this part if you want.  I've made my own library that so far contains the QG, QE, JM, AW/AC.  Will continue to add to it and make it available to everyone if desired.


Aaron
0 Kudos
Reply