Has Freescale Considered a 20 pin HCS08QG8 Part

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Has Freescale Considered a 20 pin HCS08QG8 Part

5,217 Views
Davo
Contributor II
I have used the 9S08QG8 in a few designs now.  I always find the part to be shorty by just a few pins. It woud be great if there was a 20 pin part that just had a few more I/O ports.  The HC08 and 705 lines had such parts.
Labels (1)
0 Kudos
Reply
7 Replies

2,985 Views
celsoken
Contributor V
Count me in. I currently have a lot of QG8 designs and some are already requiring extra pins. I remember legacy HC705J1A part wich was a huge Moto sucess, 20-pin pk. Good old times.

Regards,

Celso
0 Kudos
Reply

2,985 Views
peg
Senior Contributor IV
Hi,
 
I have not needed it yet, but would agree there does seem to be a big hole in the range around this size.
 
0 Kudos
Reply

2,985 Views
petr
Contributor I
Have a look at the upcomming SG part.
Petr
0 Kudos
Reply

2,985 Views
Davo
Contributor II
The SG part looks great. Any idea when it will be available ?  Is a pre-release data sheet available ?
0 Kudos
Reply

2,985 Views
celsoken
Contributor V
SG, EL, SL are good promises, the only problem is that they are not currently available.

Regards,

Celso
0 Kudos
Reply

2,985 Views
bigmac
Specialist III
Can't seem to find preliminary data sheets for any of these new devices.  Can anyone provide links?
 
Regards,
Mac
 
0 Kudos
Reply

2,985 Views
Alban
Senior Contributor II
Hello,

I used Freescale Keyword search on "MC9S08QG8"
When I say that this search is efficient... It even shows you what is not adverstised !

http://www.freescale.com/webapp/sps/site/overview.jsp?code=LPMC9S08SG

Enjoy,
Alban.


Message Edited by Alban on 2007-07-17 08:52 AM
0 Kudos
Reply