HSC08 assembly code

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

HSC08 assembly code

3,338 次查看
hityou123
Contributor II

I am doing assembly after a long time. Need some guidance -

 

To load HX register from RAM,

 

I do LDHX ram. This should load (ram) to X and (ram+1) to H

correct?

 

I am trying to write code for a clock. I increment "RTCSEC" . When the value is 30d, that's equal to 30seconds.

At every 30secs, I increment RTCMIN. When RTCMIN is 120, I increment RTCHR. If the RTCMIN is not equal to 120, the code branches to incRTCMIN.

Is this correct?

 

inc RTCSEC

lda RTCSEC

cmp #$1E ; 30 seconds

beq incRTCMIN

What to put here???

 

  incRTCMIN: clr RTCSEC

                     inc RTCMIN

                     lda RTCMIN

                     cmp #$78 ; 120 mins make an hour (since 30 secs make a min)

                     beq incRTCHR

                     bra incRTCMIN

标签 (1)
4 回复数

2,971 次查看
bigmac
Specialist III

Hello Derrick,

The assembly code for an "incrementing" solution might be as follows:

  ORG  Z_RAMStart

...

RTCSEC:   DS.B  1

RTCMIN:   DS.B  1

RTCHR:    DS.B  1

  ORG  ROMStart

...

; Increment RTC registers

RTC_INCR: INC   RTCSEC

          LDA   RTCSEC

          CMP   #30

          BLO   RI1

          CLR   RTCSEC

          INC   RTCMIN

          LDA   RTCMIN

          CMP   #120

          BLO   RI1

          CLR   RTCMIN

          INC   RTCHR

RI1:      RTS

Decimal (rather than hexadecimal) constants may be used within the code, where these make more sense.  If you are using a timer interrupt, the above subroutine could be called from within the associated ISR.

Regards,

Mac

0 项奖励
回复

2,971 次查看
Derrick
NXP Employee
NXP Employee

It's the other way around:

        ldhx    RAM     ; H = (RAM) and X = (RAM + 1)

As for your code stub, I'm going to guess that this will be run as part of an interrupt service routine (ISR) that gets executed once a second(?).  Make sure that you clear the source of the interrupt before you exit the ISR.  I'm not sure why you're only counting to 30 seconds, but I'm guessing that you don't need to display these values.  If that's the case, decrementing variables can be more efficient.  If I assume that this is correct, and that your variables are located in direct page, I suggest considering something like this:


INIT_RTCSEC:    equ     $1E                     ; initial value for RTCSEC = 30

INIT_RTCMIN:    equ     $78                     ; initial value for RTCMIN = 120


init_clock:

        mov     #INIT_RTCSEC, RTCSEC            ; initialize RTCSEC

        mov     #INIT_RTCMIN, RTCMIN            ; initialize RTCMIN

        rts                                     ; return


ISR_clock:

;

; clear the source of the interrupt

;

        dbnz    RTCSEC, ISR_clock_exit          ; decrement RTCSEC and exit if it's not zero

        mov     #$1E, RTCSEC                    ; else, reload RTCSEC with 30

        dbnz    RTCMIN, ISR_clock_exit          ; decrement RTCMIN and exit if not zero

        mov     #$78, RTCMIN                    ; else, reload RTCMIN with 120

        inc     RTCHR                           ; advance RTCHR

ISR_clock_exit:

        rti                                     ; exit

I hope that this helps.

Best Regards,

Derrick

2,971 次查看
hityou123
Contributor II

Derrick,

In the HX register, H is the MSByte and X is the LSbyte?

The HCS08 is big endian? unlike the 8085 which is little endian.

One more question -

How do I move a value to RAM ?

Mov #$02, RAM_location

0 项奖励
回复

2,971 次查看
Derrick
NXP Employee
NXP Employee

Yes, H is the MSB and X is the LSB of the 16-bit Index Register.

The endian is the opposite of the 8085. This makes it a little easier to see 16- and 32-bit values in a memory dump (but everyone has their own preferences).

Using the MOV instruction requires that either the source address and/or the destination address be in the Direct Page (i.e., 0x0000 to 0x00FF inclusive). This is why it works when accessing (most) peripheral registers. So your value in RAM needs to be located in the Direct Page for your example to work.

Best Regards,

Derrick

(I apologize for the late response - I had a busy holiday season :smileyhappy:)