HCSO8 Skipping over important code for no reason

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HCSO8 Skipping over important code for no reason

3,097 Views
mjcoury
Contributor I
So I have a routine here to catch the start of a RS232 stream....

Code:
  #ifdef USB_LOGGER  if(cSCI1rxFlag)                   // Rx Flag  {                        if( !(cSystemFlag & GWF_SCIDP) )            // If device not present    {      USBFileOpen("test.txt");                  // Open File      cSystemFlag |= GWF_SCIDP;                 // Set Device Present    }    if( !(cSystemFlag & GWF_SCIRX) )            // If we are not admist a burst    {      iUSBSendCommand(MC_e,NULL);      cSystemFlag |= GWF_SCIRX;                 // Set that we are in a burst    }    cSCI1rxFlag = 0;                            // Clear the Rx Flag    }

 
the Routine iUSBSendCommand(MC_e,NULL); gets skipped.... its output does not show up on the logic analyzer and when I step through it in processor expert, skips over that line like it does not exist.

I know that the code is inside that if routine AND that the routine works because in a 1 second loop I put


Code:
   if(cSystemFlag & GWF_SCIRX)            // If we are not admist a burst    {      iUSBSendCommand(MC_e,NULL);    }

 
And the code works as expected, I have killed almost the whole day on this :smileysad: WTF?
Labels (1)
0 Kudos
Reply
3 Replies

1,693 Views
bigmac
Specialist III
Hello,
 
I wonder if the GWF_SCIRX bit within cSystemFlag is already set when you reach that section of the code.  Following execution of the function the flag bit becomes set, and this would prevent further execution until the flag was cleared.
 
Regards,
Mac
 
0 Kudos
Reply

1,693 Views
Witztronics
Contributor IV
You need to verify that this code is not being stripped out by the compiler due to it not being used.
 
I've had routines that I thought should be there, but the compiler removed them because that section of code would always be skipped due to code errors.  It still shows up in the debugger, but gets skipped because it doesn't really exits in the executed code.
 
0 Kudos
Reply

1,693 Views
CompilerGuru
NXP Employee
NXP Employee
I would recommend to have a look to the preprocessor output and to the disassembly listing at that code position.
Those two listings can be created with the context menu in the CW ide, I always check them first when I see some unexpected behavior.
With the current information the problem could be just about anywhere, so really not enough information. The code looks basically ok, but as it is only a non complete code snippet, there are many reasons why it would not work as expected.

Daniel
0 Kudos
Reply