HCS08 detecting LVD reset even though LVD is not enabled

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HCS08 detecting LVD reset even though LVD is not enabled

1,377 Views
prasad1
Contributor II

Hi,

I am currently working on MC9S08SG8 microcontroller from HCS08 family. I have disabled Low voltage detection logic with SPMSC1 = 0; and SPMSC2 = 0. But after doing power on and off sometimes I see only LVD bit in SRS register is set(POR bit is not set) . But S08 microcontroller did not go through a reset. I am not able to understand this.Can anyone please help me to understand this behaviour?

Thanks,

Prasad

Tags (2)
1 Reply

755 Views
Fidel
Contributor IV

Hello, your issue is closed or not? if closed ,then what is the root cause? or anybody can help on this? I also met the same issue recently, thanks a lot~