HCS08 and SPI flash - HCS08QE8

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

HCS08 and SPI flash - HCS08QE8

2,346 次查看
jag
Contributor IV
Hello,
I neeed to implement the communication between a HCS08QE8 and an Atmel serial DataFlash (AT25DF321) using the SPI port.
So, before trying to reinvet the wheel, I thought to ask here if someone has already written the code necessary (hopefully in C) and wish to share it with me :smileyhappy:

Thanks Bye Jack
 
 
 
 
 
Added p/n to subject.


Message Edited by NLFSJ on 2008-10-17 02:00 PM
标签 (1)
0 项奖励
回复
2 回复数

1,017 次查看
Witztronics
Contributor IV
Here is one that I wrote for an Intel SPI flash.  These flash routines should be a helpful starting place.

The original code used Processor Expert to generate the SPI routines.
0 项奖励
回复

1,017 次查看
jag
Contributor IV
Thanks!

Bye Jack
0 项奖励
回复