HCS08 - Unrequest break on interrupt

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

HCS08 - Unrequest break on interrupt

3,945 次查看
Richard777
Contributor I
Hi guys, I'm using the CodeWarrior for HCS08 and debug with P&E BDM Multilink, my problem is that when debbugin my application the debbuger stop execution on interrupt vector ( SCI in my case ) and haven't breakpoint in this ISR !. Exists a way to eliminate this behavior?
Thanks in advance !

 
 
 
 
 
 
 
 
 
Added product family to subject.


Message Edited by NLFSJ on 2007-06-22 03:49 PM
标签 (1)
0 项奖励
回复
5 回复数

2,242 次查看
peg
Senior Contributor IV
Hi Richard,
 
When EXACTLY does it break?
Can you simply restart it and it carries on?
Or is it truly broken?
 
0 项奖励
回复

2,242 次查看
Richard777
Contributor I
Hi Peg,
 
>When EXACTLY does it break?
Break after routine of transmition
>Can you simply restart it and it carries on?
This happend.
 
Thanks !
0 项奖励
回复

2,242 次查看
Alban
Senior Contributor II
Hello,

Is there an error message in the spirit of "Illegal Breakpoint" ?
Or any other indication.

Regards,
Alban.
0 项奖励
回复

2,242 次查看
bigmac
Specialist III
This seem to be a split thread with the Codewarrior 8- and 16-bit forum.
 


Message Edited by bigmac on 2007-06-27 12:01 PM
0 项奖励
回复

2,242 次查看
Alban
Senior Contributor II
Thanks Mac, I was just realizing.

Thread locked.

PLEASE, again Do NOT Crosspost, a good example here on how to waste time :smileysad:
0 项奖励
回复