HCS08 - Unrequest break on interrupt

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HCS08 - Unrequest break on interrupt

3,931件の閲覧回数
Richard777
Contributor I
Hi guys, I'm using the CodeWarrior for HCS08 and debug with P&E BDM Multilink, my problem is that when debbugin my application the debbuger stop execution on interrupt vector ( SCI in my case ) and haven't breakpoint in this ISR !. Exists a way to eliminate this behavior?
Thanks in advance !

 
 
 
 
 
 
 
 
 
Added product family to subject.


Message Edited by NLFSJ on 2007-06-22 03:49 PM
ラベル(1)
0 件の賞賛
返信
5 返答(返信)

2,228件の閲覧回数
peg
Senior Contributor IV
Hi Richard,
 
When EXACTLY does it break?
Can you simply restart it and it carries on?
Or is it truly broken?
 
0 件の賞賛
返信

2,228件の閲覧回数
Richard777
Contributor I
Hi Peg,
 
>When EXACTLY does it break?
Break after routine of transmition
>Can you simply restart it and it carries on?
This happend.
 
Thanks !
0 件の賞賛
返信

2,228件の閲覧回数
Alban
Senior Contributor II
Hello,

Is there an error message in the spirit of "Illegal Breakpoint" ?
Or any other indication.

Regards,
Alban.
0 件の賞賛
返信

2,228件の閲覧回数
bigmac
Specialist III
This seem to be a split thread with the Codewarrior 8- and 16-bit forum.
 


Message Edited by bigmac on 2007-06-27 12:01 PM
0 件の賞賛
返信

2,228件の閲覧回数
Alban
Senior Contributor II
Thanks Mac, I was just realizing.

Thread locked.

PLEASE, again Do NOT Crosspost, a good example here on how to waste time :smileysad:
0 件の賞賛
返信