HCS08 : 3.3v MCU and 5v logic ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

HCS08 : 3.3v MCU and 5v logic ?

8,485 次查看
BC109
Contributor I
Hi,

I'm a brand new user of HCS08 family (HCS08QG8). This MCU is running at 3.3v, and I have no experience about how to connect 5v peripherals. I was previously using HC11 at 5v.

I read lots of things about 5v-tolerant inputs, direct-driving of 5v inputs from 3.3v outputs, and various level converters (74LVC, 74ALVT, etc...) As I'm completely novice with 3.3v logic, could someone point me out some kind of tutorial or 3.3v beginner's guide in relation with HCS08 MCU ?

Also, are there anny Application Notes about that ?

Thank you in advance,
Toussaint OTTAVI
标签 (1)
0 项奖励
回复
7 回复数

2,177 次查看
BC109
Contributor I
Hi,

Thank you everybody for the answers.

Of course, the perfect MCU for me would be a QG8 with the 5v capability of the AW family, and with the 'HC11 full assembly language. Hey, Mr Freescale, could you build it for me ? :smileyhappy:

It's only for small amateur applications, and in most of the cases, I will need very few I/O, that's why the QG8 PDIP package is perfect, because it avoids complex PCB design using high pin count devices.

Thanks again for the help, I'll try to play around with it ASAP.

Best regards from Corsica,
Toussaint
(ham radio, TK1BI)
0 项奖励
回复

2,177 次查看
Nabla69
Contributor V
Hi Toussaint,

Please let me add my two cents worth.
There is AN2433 - 5V to 3V Considerations that I could recommend reading.

Cheers,
Alvin.

(Alban fixed link)

Message Edited by Alban on 05-09-2006 10:51 AM

0 项奖励
回复

2,177 次查看
UK_CF_FAE
NXP Employee
NXP Employee
Guys - check out the MC9S08AW family of parts (16k to 60k flash) which are 1.8 to 5.5 volt operation.
 
OK, a bit larger packages than the QG8. But fully featured. What will you do with those 2-off SCI UARTs?
 
Mark
 
 
 
 

Message Edited by UK_CF_FAE on 05-10-200603:15 PM

0 项奖励
回复

2,177 次查看
bigmac
Specialist III

Hello Toussaint,

Provided you don't need a lot of speed, the use of open drain N-channel MOSFETs might be suitable.  The MOSFET type should be capable of switching with 3V logic levels at its gate (and would also suitable for 5V levels).  The drain would connect to the logic input, and  would also require a suitable pull-up resistor to either 3V or 5V, depending on the conversion direction.  The resistor value will depend to some extent on the speed you require.

Of course your code will need to allow for inverted polarity through the device.

An alternative to the MOSFET could be the use of bi-polar NPN transistors, but these would need an additional resistor in series with the base.

Regards,
Mac

 

0 项奖励
回复

2,177 次查看
BobMac
Contributor I
Hi there, BC 109. I had the same problem when faced with talking to some SD memory modules. As I remember, TI has a great app note on just this subject of voltage level shifting. I can't find my old notes now, but I sure remember the source because of my frustration at the time.
Regards, Bob

PS, I have a "HAM" license and in the early 1950's I owned a Military radio out of a B17, the BC628. It used tubes (vacuum state) but worked quite well, as I remember.
0 项奖励
回复

2,177 次查看
rocco
Senior Contributor II
Hello, Toussaint:

Welcome to the world of mixed voltages. I avoided 3 volts for years, because of the very issues you express now. I finally had to take the plunge when Motorola discontinues the DSP56002, and replaced it with the 3 volt DSP56303. But at least the DSP56303 had many 5 volt-tolerant I/Os.

Here are two tricks that I learned:
You can use 74HCTxxx parts as buffers to turn 3 volt outputs into 5 volt outputs. The 74HCT parts use TTL-level input thresholds, which are near 2 volts for the minimum high state, and 3 volts outputs can satisfy that threshold.

Terminating resistor packs, often used in SCSI systems, make excellent voltage divides. Specifically, the packs that contain 220ohm/330ohm pairs. 5 volts in becomes 3 volts out. A disadvantage is that it puts a hefty (550ohm) load on the 5 volt output, and it will increase propagation delay if the 3 volt input has a capacitive component.

Then again, there are chips designed specifically for your problem.

The simplest approach, though not always feasible, it to switch everything over to 3 volts.
0 项奖励
回复

2,177 次查看
glork
Contributor I


BC 109 wrote:
Hi,

I'm a brand new user of HCS08 family (HCS08QG8). This MCU is running at 3.3v, and I have no experience about how to connect 5v peripherals. I was previously using HC11 at 5v.

I read lots of things about 5v-tolerant inputs, direct-driving of 5v inputs from 3.3v outputs, and various level converters (74LVC, 74ALVT, etc...) As I'm completely novice with 3.3v logic, could someone point me out some kind of tutorial or 3.3v beginner's guide in relation with HCS08 MCU ?

Also, are there anny Application Notes about that ?

Thank you in advance,
Toussaint OTTAVI




Good morning.
Although Freescale makes some 3.3V devices which are 5V tolerant on some I/Os the 9S08QG family isn't amoung them. If you must use this device with 5V peripherals you will need to use appropriate level conversion circuitry.
Sorry, I'm not aware of any tutorials on the use of 3.3V logic but a google search might turn up some.
ron
0 项奖励
回复