HC11E2...Windows Interface to download to EEPROM?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HC11E2...Windows Interface to download to EEPROM?

1,559 Views
Will_CalPoly
Contributor I

Hi,

I know I'm using some really old equipment, but its what we have to work with at school for this project. I am looking for a program, hopefully free, so that I can download to my EEPROM using Windows. I have an old 386 in the lab I'm working in that has Dunfield's MicroC, but the thing works with a 5.25" floppy and its extremely difficult to be productive on. I am using a Mini Board 2.0 from MIT that I guess was used in the early 90's. The documentation is non-existent anymore because the MIT ftp site for the board has been down for years. Any help would be greatly appreciated. I'm using MiniIDE right now with an asm11 assembler, but I'm not having any luck communicating with the board using this set up. Thanks,

 

Will

Labels (1)
0 Kudos
Reply
1 Reply

980 Views
RogerSchaefer
Contributor III

If you are using a old 386 then PCBUG11 will work.  With faster computers use JBUG.

 

Check out my webpage http://www.rasmicro.com/

 

Roger

0 Kudos
Reply