HC11 or HC12 help libraries

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

HC11 or HC12 help libraries

1,796 次查看
student
Contributor I
Hi,
i am a student who need to connect a microprocesor to an IC devices which i need to configure throught an I2C or SPI bus. i can use either the MC68HC11 (writting in assembly using Bufflao compiler) or the MC68HC12 (writing using codewarrior).
Are there any libraries that i can add to the compilers so it is easier to use any of this buses (i only need to use one of them, depending on your answer...).?
Are these libraries free/how much does they cost?
Where can iu find this libraries?
 
Thanks
标签 (1)
0 项奖励
回复
1 回复

1,107 次查看
Alban
Senior Contributor II
Hello Student,

I would advise to use the HC12, it is simpler, I think.
In your CodeWarrior, look for Processor Expert and see if it supports your product.

You have modules available on their website and it does most of the work for you
- init routines,
- read/write interrupt sub-routines (ISR)...

CodeWarrior is FREE for this size of application and Processor Expert is included in CodeWarrior.
You may want to get the latest CodeWarrior.


CodeWarrior Development Studio for HC12 Microcontrollers
Evaluation Software Version - Evaluation license required. See info icon for more information.   
FREESCALE  exe  342907  4.6  


Cheers,
Alban.
0 项奖励
回复