HC08QC8 programming issue with P&E Multilink

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HC08QC8 programming issue with P&E Multilink

2,507 Views
TonyLin
Contributor I
Hi, I am using a P&E Multilink to program code into QC8 chip. However, I always encounter this problem during flashing procedure.
"Trying Security $FFFFFFFFFFFFFFFF Access Denied.
   (68HC08 Device responded properly, but ROM is secure.)
ERROR 48 during script!"
 
It is not caused by my program, because I use CodeWarrior to generate a fresh new QC8 code to try.
But if I only change the device setting to QC4 or QY4, the flashing works.
 
Is there any compatibity issue between Multilink and QC8? Thanks!
Labels (1)
0 Kudos
Reply
2 Replies

1,562 Views
Alban
Senior Contributor II
Hello,
 
You need to make sure you have a Power On Reset (power cut and put back on).
And you can ignore security to erase the flash.
 
Regards,
Alban.
0 Kudos
Reply

1,562 Views
peg
Senior Contributor IV
Hi Tony,
 
Given that the only real difference between a QC4 and a QC8 is the amount of flash and that the QC4 setting works, I would assume there is a problem with the 08P file for the QC8. The only problem with using a QC4 file on a QC8 should be that you are limited to the top half of the FLASH.
You could try hunting down a more up to date version of the programming algorithm on www.pemicro.com
or putting this question direct to them on their forum there.
 
0 Kudos
Reply