HC08LK code size problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

HC08LK code size problem

2,466 次查看
alzomor
Contributor I

Hi

 

I am uing HC08LK family.

Now my code size exceeds the 24K Flash.

Is there any rplacment with more flash size 32K or 64K.

I am looking for the replacemnt micro which requires the least changes in my source code and HW design

 

Best Regards

Hossam Alzomor

标签 (1)
0 项奖励
回复
3 回复数

1,648 次查看
bigmac
Specialist III

Hello Hossam,

 

If the HC908LK24 device was originally chosen because of its LCD drive capability, you might wish to examine the datasheet for the more recent HCS08LC60.  This is a member of the newer HCS08 family.

 

I have not compared the two pinouts, but I suspect that it will be quite unlikely that they are similar to each other.

 

With regard to coding, that associated with all on-chip peripherals will certainly need to be modified, to be consistent with the register naming, and for compatibility with the operation details of each peripheral.

 

Regards,

Mac

 

0 项奖励
回复

1,648 次查看
alzomor
Contributor I

Dear Mac,

 

Is there any Application note for megiration from LK24 to LC60?

 

Best Regards

Hossam Alzomor

0 项奖励
回复

1,648 次查看
bigmac
Specialist III

Hello Hossam,

 

I am unfamiliar with the application notes that may pertain to the 'LC60.  However, if you examine the products section of the Freescale website, you can drill down to the webpage containing specific information about the 'LC60 device.  Here you will generally find a list of all the application notes that pertain to that product, and can download the documents from that webpage.

 

Regards,

Mac

 

0 项奖励
回复