Go into sleep mode when there is no coordinator - MC13213

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Go into sleep mode when there is no coordinator - MC13213

1,779件の閲覧回数
Nicolas_martel
Contributor I

Hello all,

 

I want to know if it's possible for a End device to go into sleep mode when there is no coordinator?

I use a MC13213.

 

If it's possible !  How do that ?

 

 

Added p/n to subject.

Message Edited by NLFSJ on 2009-04-01 03:36 PM
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

973件の閲覧回数
Nicolas_martel
Contributor I
Nobody knows if this is possible?

Nobody knows what is the variable which must be changed in Beekit or CodeWarrior?

 

How go in sleep mode when there is no coordinator ?

 

 

0 件の賞賛
返信

973件の閲覧回数
Nicolas_martel
Contributor I
My sequence is :
My coordinator and my end device are ON (turn on). My end device work with a battery (3V).
When I press the switch (end device) the LED of coordintor turn on. And after the end device enters in sleep mode.
After that I turn off my coordinator. If I press my switch, the of coordinator turn off. It's normal.
But my end device don't enter in sleep mode. Why my end device don't enter in sleep mode when my coordintor is turn off ?
0 件の賞賛
返信