Ghost effect on Custom LCD

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Ghost effect on Custom LCD

2,859件の閲覧回数
longliveboy
Contributor I

Hi everybody;

 

I'm working on a LCD but there is a ghost effect on passive segments. on the other hand when i change viewing angle all segmets appears.

 

IC is LL64

lcd frequency is 64Hz also lcd capacitance is 35800pF.

This values are so far away that LL16 support but i wanna know ghost effect causes from which conflict? 

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,874件の閲覧回数
BasePointer
Contributor II

For ghost effect: try reducing refresh rate to 30Hz.

 

For "all segmets appears": try reducing contrast and use lowest bias mode possible, for example 1/3 bias mode. 1/2 bias mode is bad at contast ratio.

 

0 件の賞賛
返信

1,874件の閲覧回数
longliveboy
Contributor I

Hi BasePointer;

 

i already try all freaquency ranges but result is same.

bias is fix at 1/3

 

do u know is TN lcds are couses this problem.

i know tn's viewing angle is too narrow but cant guess that it is as bad as mine.

 

already thanks

0 件の賞賛
返信

1,874件の閲覧回数
BasePointer
Contributor II

Hi,

 

Yes also low quality TN glasses can cause this problem. Try contacting your custom LCD manufacturer and ask for LCD parameters. We did many sample requests from the manufacturer in the past to find perfect lcd solution that has TN glass.

 

Also dont forget, multiplexing reduces total required pin count but it reduces contrast ratio too. We are using 4x40 = 160 segments custom LCD and TN glass without problem. (no ghost effect, wide range viewing angle) We need totally 44 pins. We could also choose 8x20 (28 pins) = 160 segments LCD but, it would have worse contrast ratio.

 

If you don't have price, industrial temperature range and life time problems, you can choose HTN or STN glass types.

 

BP. 

0 件の賞賛
返信