Gang Programmer for HC08

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Gang Programmer for HC08

4,519 Views
glork
Contributor I
Hello.
I'm looking for a (say 4-) gang programmer for the 68HC908QY4 dip processor for production use. Anyone know a source, have experience??
Thanks in advance.
ron
Labels (1)
0 Kudos
Reply
2 Replies

2,343 Views
HonHo
Contributor I
We are SofTec Microsystems, a famous European company which specialize to develop hardware debuggers and programmers for Freescale microcontrollers.
 
If you consider to have socket programming, I would suggest you to have a look on our MP8011A gang programmer (1 to 8).
 
On the other hand, we are also provide in-circuit programming solution, inDART-One. It is a gangable in-circuit programmer AND debugger for HC08/HCS08/HCS12(X)/RS08 families. InDART-One also provides unique FAST PROGRAMMING algorithm to increase the programming speed.
 
For more information, please visit the following links respectively.
 
 
Thank you.

Message Edited by Hon Ho on 2006-11-2411:24 AM

0 Kudos
Reply

2,343 Views
jah
Contributor I
consider
tribalmicro.com
ALL-GANG Gang Programmer
http://www.tribalmicro.com/all-gang/
you will need a base unit + 4 or 8 position head + socket adapter


also consider the cyclone from pemicro.com, granted not a 4head unit but costing lo enough to buy 4units and a usb hub.
0 Kudos
Reply