GT16A I2C interface with MAX1069

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GT16A I2C interface with MAX1069

2,732 Views
woohoo
Contributor I

Hi,

 

I am trying to use the I2C interface for the first time and am unsure of my code. I am using the GT16A as a master and am attempting to read data from the MAX1069 14 bit ADC IC. Below is my I2C initialising function and the read function. I am not getting the results I expected and I am unsure why. Any help will be greatly appreciated! edit->Turns out I forgot the pull-up resistors, but I still can't get the ADC to function correctly..

 

   int receiveIIC (void) // Thermistor ADC - MAX1069    {     byte dataADC[2] ;     int result;     unsigned char MAX_delay = 100;     unsigned int count;          IICC_IICEN = 1; // IIC enabled     IICC_TX = 1; // Set Transmit     IICC_MST = 1; // Set START          // Send address. LSB decides on R or W     while(IICS_TCF == 0);     IICD = 0x61;  // Address -> 0110000, LSB for receive -> 1 = 0x61          // Address -> 0110000, LSB for receive -> 0 = 0x60    for (count=0;count<MAX_delay;count++) asm("nop");           while(IICS_TCF == 0);     IICC_TX = 0;          dataADC[0] = IICD; // Receive first byte      for (count=0; count<MAX_delay;count++) asm("nop");     while(IICS_TCF == 0);          IICC_TXAK = 1;  // Send No Acknowledge     dataADC[1] = IICD; // receive second byte     for (count=0; count<MAX_delay;count++) asm("nop");     while(IICS_TCF == 0);          IICC = 0x80;              result = dataADC[0] << 8;          result += dataADC[1];                            return result;     }
Labels (1)
Tags (5)
0 Kudos
Reply
4 Replies

2,512 Views
Monica
Senior Contributor III

Hello Oliver!

How is the project going?

We'd like to know if this suggestion was helpful throughout your problem, would you share with us?

Best regards,

Monica.

0 Kudos
Reply

2,512 Views
weapon
Senior Contributor I

Hi Hobson,

There is a AN to show you how to use IIC in hcs08, hope it is useful.

http://cache.freescale.com/files/microcontrollers/doc/app_note/AN3291.pdf

And just take a look at your code, I think there are three problems.

1. You didn't check ACK from slave.

2. There are some problems after transimiting slave address

  • // Send address. LSB decides on R or W  
  •  
  • while(IICS_TCF == 0);  
  •  
  • IICD = 0x61;  
  • // Address -> 0110000, LSB for receive -> 1 = 0x61  
  •  
  • // Address -> 0110000, LSB for receive -> 0 = 0x60  
  •  
  • for (count=0;count<MAX_delay;count++) asm("nop");  
  •   
  • while(IICS_TCF == 0);   //  waiting the slave address sending out
  • while(IICS_RXAK == 1);  // wait ack
  • IICC_TX = 0;  
  • (void)IICD; // dummy read to clear TCF flag; this step is important,becuase TCF was set after the slave address was sent.
  • while(IICS_TCF == 0);  // then wait for the first byte coming
  • dataADC[0] = IICD;

3. result = dataADC[0] << 8;   I don't think that is a good practice to shift like that. dataADC[0] is a 8-bit data, your practice is depending on compiler's implicit cast. the good practice is to do cast by ourselves. like that:

    result = (int)dataADC[0] << 8;

Hope my answers is helpful.

   

.

0 Kudos
Reply

2,512 Views
woohoo
Contributor I

So I started to attempt to write the I2C send routine that will communicate with a 14 bit, AD5647R DAC. I have encountered a problem where the high bit for the data is missing the front 2 zeroes after I split the incoming value. I have done this as shown below. Any ideas? Also still haven't managed to get the read function to work... edit->It is working with the code below now

void sendIIC (int output)

{

  byte dataDAC[2];

  unsigned char MAX_delay = 100;

  unsigned int count;

  dataDAC[0] = (output>>8) & 0x00FF; // High

  dataDAC[1] = (output) & 0x00FF; // Low

  IICC_IICEN = 1; // IIC enabled

  IICC_TX = 1; // Set Transmit

  IICC_MST = 1; // Set START

  // Send address. LSB decides on R or W

  while(IICS_TCF == 0);

  IICD = 0x1E; // Address -> 0001111, LSB for receive -> 0

  for (count=0; count<MAX_delay;count++) asm("nop");

  // Send Command byte

  while(IICS_TCF == 0);

  IICD = 0x1F; // Command: R->0 ,S->0 ,Command->011 (Write to and update DAC n) ,DAC Address->111 (Both DACs)

  for (count=0; count<MAX_delay;count++) asm("nop");

  // Send high data byte

  while(IICS_TCF == 0);

  IICD = dataDAC[0]; // Send the high bits

  for (count=0; count<MAX_delay;count++) asm("nop");

  // Send low data byte

  while(IICS_TCF == 0);

  IICD = dataDAC[1]; // Send the low bits

  for (count=0; count<MAX_delay;count++) asm("nop");

  IICC = 0x80;

}

0 Kudos
Reply

2,512 Views
weapon
Senior Contributor I

Hi Hobson,

The send function's problem is just like receving function. you didn't wait slave's ACK. and at the last, you'd better  polling IICS_TCF to confirm dataDAC[1]'s transfer is completed.

IICD = dataDAC[1]; // Send the low bits    

for (count=0; count<MAX_delay;count++) asm("nop");  

while(IICS_TCF == 0);

IICC = 0x80;  


0 Kudos
Reply