Frequency at 1.8V & EEPROM Emulation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Frequency at 1.8V & EEPROM Emulation

2,596 Views
suzanne_lim
Contributor I
I'm interested in developing a prototype with MC9S08QE8CWL but i have 2 question to clarify before i start.

1.What is the frequency of the chip if the chip voltage is 1.8V? Can anyone provide me with the frequency graph vs voltage?

2.I can't find any document & source code to help me with EEPROM Emulation. Can anyone point me the link?
Thanks:smileyhappy:
Labels (1)
0 Kudos
Reply
3 Replies

1,740 Views
Ake
Contributor III
Hi,
I answered your questions thru the Freescale CRM.
 
Was there something wrong with the answer?
 
I am just curious.
 
Regards,
Ake
0 Kudos
Reply

1,740 Views
suzanne_lim
Contributor I
Nope! there's nothing wrong. I posted two at the same time to get the answer faster. Thanks for the answer

for all,

The answer by AKE is

1) The operating voltage is 1.8 V - 3.6 V. Within that span, the
component behaves normally, so no compensation is needed.
See Section 3.13 and Table 7 in MC9S08QE8.

2) I have no paper describing the 9S08QE8. The closest I got is the
9S08QG8, so I will send you a paper/file describing that MCU instead.




0 Kudos
Reply

1,740 Views
Ake
Contributor III
Hi,
Thanks! I got the feeling that I had made a fool of myself by sending something useless.
 
Have a nice day,
Ake
0 Kudos
Reply