Freescale equivelant to AVR ATtiny2313

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Freescale equivelant to AVR ATtiny2313

4,722 Views
RichT
Contributor I
Hi
 
I find the freescale product selector guides very confusing, is it just me? :smileywink:  I am trying to find a freescale part similar to an AVR ATtiny2313.  The important parts are cheap, 5V operation and at least 13 GPIO lines in a DIP style package that is in circuit programmable/debug-able preferably using the USB BDM pod rather than the multilinker/cyclone aproach which I find infuriating on the QT4.  Is there such a beast ?  oh, no need for AD etc though PWM would be nice as would a small eeprom for storing settings > 10000 times.  Are there any better selection guides for the freescale 8bit parts, they don't appear to be able to filter by 5V or IO as a primary search, seems like trial and error. 
 
Thanks for your time
 
Rich
 
PS. 
Labels (1)
0 Kudos
Reply
3 Replies

1,034 Views
bigmac
Specialist III

To my knowledge, there are currently no low pin count parts (available in DIP) that will operate from 5 volts, and use BDM.  The closest device to meet the majority of your requirements would be the 9S08QG4/8, but this is 3.3 volt maximum.  You will need to use flash for your non-volatile data storage requirements.

Regards,
Mac

 

0 Kudos
Reply

1,034 Views
peg
Senior Contributor IV

Hi Rich,

Also the P&E manufactured adapter for BDM is still called Multilink and Cyclone. The main thing I believe you are trying to differentiate between is MON08 with QT/QY and BDM with QG for example.

Regards David

 

0 Kudos
Reply

1,034 Views
RichT
Contributor I
Thanks Mac, that device does look interesting and would allow me to use exisiting dev tools :smileyhappy:  shame its 3V but I can maybe live with that.  It is more expensive that the AVR too.   Think I'll grab one and take a look, thanks!
 
David, you are correct, my bad.  It has been a couple of years since I looked at the QT4 with MON08 vs the BDM system on GB60 etc.
 
thanks guys.
 
Rich
 
0 Kudos
Reply