Freescale Wireless Demo

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Freescale Wireless Demo

3,392件の閲覧回数
datamstr
Contributor II
Hi all,
I went to a Freescale wireless seminar in Michigan about a year ago. We used a small demo board in the lab tests and I am having a difficult time locating that demo board on the Freescale site. I think the demo board has both an 8 bit MPU and the wireless chip on it. Basically, I only need to run a simple field test in a factory for range and dead spots. The resulting functionality I will need is to send 1-4 bytes of data to a mobile cart using wireless.
So, I have a few questions for the group:
1. What is that demo board part number and is it available?
2. Can I just use the wireless chips in a "test mode" where just the "carrier" is transmitted to a receiver and do something like light up a LED if signal is present?
3. Any other suggestions on making a simple site test?

Thanks so much!
David
ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,906件の閲覧回数
datamstr
Contributor II
Hi Peg,

The MC13192DSK might be the demo we used, but I thought it had a USB connector on it.
Also, thanks for the link to the range testing information.
I will check the datasheet to see if I can run a test with just the radio, but no MPU.
Thanks,
David
0 件の賞賛
返信

1,906件の閲覧回数
ok2ucx
Contributor IV
Hi, you may be looking for ZSTAR demo, fully documented here:
 
 
Regards, Pavel, ok2ucx
0 件の賞賛
返信

1,906件の閲覧回数
peg
Senior Contributor IV
0 件の賞賛
返信