Freescale 802.15.4 MAC???

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Freescale 802.15.4 MAC???

2,785件の閲覧回数
admin
Specialist II

I have bassically two questions about the full (not the SMAC) Freescale 802.15.4 MAC:

 

1. Is there a way to know how many MAC retries has been used to transmit a message?

 

2. If a radio receive two times the same packet (in the case the  first ack was send but not receive by the transmitter), is the second packet discard by the MAC layer? If not, is there a way to have access to the sequence number of the received packet?

 

Thanks in advance for your help!

Fred

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,737件の閲覧回数
xiaof
Contributor I
2. the second packet will be discard by the MAC layer,because those two packets have the same sequence number.
0 件の賞賛
返信

1,737件の閲覧回数
xiaof
Contributor I

 

1. retries times is  a MAC constant:aMaxFrameRetries,it's value is 3. 

0 件の賞賛
返信

1,737件の閲覧回数
admin
Specialist II
Anyone understanding these issues?
0 件の賞賛
返信