Force a CAN TXerr

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Force a CAN TXerr

2,981 Views
Saga
Contributor II
Hi to all,

I'm working in some method to verify the sned of a CAN message when an error ocurrs, the problem i have is... How can i force a TXerr in the CAN bus to test this method, this is for certification purposes...

I'm using a DZ60 uC... Thank you a lot guys...
Labels (1)
0 Kudos
Reply
2 Replies

1,989 Views
Saga
Contributor II
Ok seems nobody knows or probably i didn't explain myself correctly... :mansad:

In the MC9S08DZ60 there is a register called:

MSCAN Transmit Error Counter (CANTXERR)

What conditions could ocurr for this register to increment?

How could i force an error that would make this register increment??
0 Kudos
Reply

1,989 Views
allawtterb
Contributor IV
I would suggest taking a look at AN2283, specifically the section on errors (Pages 24-40):
 
The document is meant for the MSCAN module used in HC08 and HC12 but I believe the error conditions are the same.  To see the differences between the HC08/12 MSCAN and HCS08 MSCAN take a look at AN2717, Section 6.7(Page 17):
 
http://www.freescale.com/files/microcontrollers/doc/app_note/AN2717.pdf?fsrch=1&WT_TYPE=Application Notes&WT_VENDOR=FREESCALE&WT_FILE_FORMAT=pdf&WT_ASSET=Documentation
 
There are 5 conditions that can cause errors, 2 that are detected by the transmitter: A Bit Error and Acknowledgement Error.  These are both described in the first document above on pages 24 and 25.
 
- Brett
 
 
 
0 Kudos
Reply