Flashed 13213-NCB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flashed 13213-NCB

2,371 Views
xinr1b488
Contributor I
Hi, i just recently flashed my 13213-NCB network coordinator board, so i was wondering is there any chance to get back the message " Welcome to SND! PAN Coordinator." on the lcd? and of course the LEDs that are lighted when the SRB within the range. the same question goes out to 13213-SRB. Sensor reference board.
Labels (1)
0 Kudos
Reply
3 Replies

1,560 Views
Mads
Contributor V
xinr1b488,
 
I think you need to elaborate a bit on what software your are running.
Our Beestack, MAC and SMAC demo applications does not display that message.
 
but if you are using an application generated from Beekit then you properly have to "enable" the display module.
 
BR,
Mads
0 Kudos
Reply

1,560 Views
xinr1b488
Contributor I
i've accidentaly flashed in the NCB, therefore it is not able to reusme it's previous functions, so is there any way to resume back the message of "Welcome to SND! PAN Coordinator." And yes, we are using the software BeeKit.
 
Thanks!
0 Kudos
Reply

1,560 Views
Mads
Contributor V
please tell me the name of the codebase you are using (and version) as non of our existing codebases prints out this message.
 
Br,
Mads
0 Kudos
Reply